Flash size for USB to serial example on EFM8UB1

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero Employee</font></font> </a> jstine on ‎03-01-2017 05:55 PM

Question

What flash size of EFM8UB1 is required to run the USB to serial example?

Answer

The example provided in Simplicity Studio compiles to 11,576 bytes (release mode, optimized for size), so the 16k part is required.