Capacitive Sense Profiler Debug Adapter Compatibility

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero Employee</font></font> </a> Alan_S on ‎12-02-2016 10:27 AM

Question

Why can't I see any raw data in the Capacitive Sense Profiler when connected to my board through a USB Debug Adapter?

Answer

The Capacitive Sense Profiler is not compatible with the USB Debug Adapter. A Toolstick Base Adapter and Toolstick Debug Adapter must be used in order to connect to custom hardware and see raw capacitive sensing data.