Reply
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Ninja</font></font> </a> tj
Posts: 46
Registered: ‎07-04-2016

rtcdriver and calendar mode

Is rtcdriver can be used with RTC in calendar mode ? Is API for calendar ?

I need IRQ every 1min and 1day, how to properly integrate it with rtcdriver ?

 

Posts: 1,733
Registered: ‎10-14-2014

Re: rtcdriver and calendar mode

@tj

As far as I know unfortunately that the RTCC is implement as normal mode (not calendar) in the rtcdriver driver code.

 

My views are my own and do not necessarily represent the views of Silicon Labs

WeiguoLu