Reply
Posts: 96
Registered: ‎08-20-2016

emwin for pearl gecko

hello 

i am using the efm32pg12 slstk3402A and i want to use the emwin library for the 128x128 sharp memory lcd.

1) i dont see any example\demo in the simplicity, attached.

2) is there an emwin example i can start with? 

 

 

Posts: 259
Registered: ‎08-16-2012

Re: emwin for pearl gecko

You can refer to AN0048, this application note is for Giant Gecko device but it can be changed to EFM32PG12.

My views are my own and do not necessarily represent the views of Silicon Labs
Posts: 96
Registered: ‎08-20-2016

Re: emwin for pearl gecko

how do i port the project to PG ?

please explain all of the steps?

 

Posts: 96
Registered: ‎08-20-2016

Re: emwin for pearl gecko

hello

i saw in the datasheets of the GG and PG that the dma is not exactly the same

the GG has dma and the PG has Ldma.

whats the different in regard of the porting?

Posts: 96
Registered: ‎08-20-2016

Re: emwin for pearl gecko

hello

as i said before, i would like to use emwin with the Pearl gecko mcu.

so i thought it would be faster to use a GG watch demo (an0048) and port it to PG.

after reviewing the an0918.0 and starting to port the GG watch demo (emwin) to PG it seems that there are alot of errors  when i build and i think that alot of changes need to be done.

i would very much appreciate if you could upload an emwin example that runs on a PG (an0048 or something else). 

thank you.