Reply
Highlighted
Posts: 65
Registered: ‎08-20-2016

emwin for pearl gecko

hello 

i am using the efm32pg12 slstk3402A and i want to use the emwin library for the 128x128 sharp memory lcd.

1) i dont see any example\demo in the simplicity, attached.

2) is there an emwin example i can start with? 

 

 

Posts: 246
Registered: ‎08-16-2012

Re: emwin for pearl gecko

You can refer to AN0048, this application note is for Giant Gecko device but it can be changed to EFM32PG12.

My views are my own and do not necessarily represent the views of Silicon Labs