Reply
Highlighted
Posts: 28
Registered: ‎08-30-2013
Accepted Solution

UART using STK3800

Hi,


I have been trying to get the UART1 functionality working on the STK3800 (Wonder Gecko) by using PD0 (Tx) and PD1 (Rx) and 1 (GND) on the expension hedaer. I have made minor changes to the code from the application note AN0045 USART or UART Asynchronous mode  (changes: Used PORTD instead of PORTB, also location of UART1 changes from 2 to 1).


For some reason, I am not able to get any communication to and from the kit. I am using FTDI USB to 3.3V TTL serial cable in order to interface it to PC using docklight serial software. I have posted my code below, please see if you can guide me in the right direction. Thanks in advance.



#include
#include
#include em_device.h
#include em_chip.h
#include em_cmu.h
#include em_gpio.h
#include em_emu.h
#include em_system.h
#include em_usart.h
#include bsp.h
#include bsp_trace.h

/* Function prototypes */
void uartSetup(void);
void cmuSetup(void);
void uartPutData(uint8_t * dataPtr, uint32_t dataLen);
uint32_t uartGetData(uint8_t * dataPtr, uint32_t dataLen);
void    uartPutChar(uint8_t charPtr);
uint8_t uartGetChar(void);

/* Declare some strings */
const char     welcomeString[]  = Energy Micro RS-232 - Please press a key
;
const char     overflowString[] =
---RX OVERFLOW---
;
const uint32_t welLen           = sizeof(welcomeString) - 1;
const uint32_t ofsLen           = sizeof(overflowString) - 1;

/* Define termination character */
#define TERMINATION_CHAR    '.'

/* Declare a circular buffer structure to use for Rx and Tx queues */
#define BUFFERSIZE          256
volatile struct circularBuffer
{
  uint8_t  data[BUFFERSIZE];  /* data buffer */
  uint32_t rdI;               /* read index */
  uint32_t wrI;               /* write index */
  uint32_t pendingBytes;      /* count of how many bytes are not yet handled */
  bool     overflow;          /* buffer overflow indicator */
} rxBuf, txBuf = { {0}, 0, 0, 0, false };

/* Setup UART1 in async mode for RS232*/
static USART_TypeDef           * uart   = UART1;
static USART_InitAsync_TypeDef uartInit = USART_INITASYNC_DEFAULT;
/******************************************************************************
 * @brief  Main function
 *
 *****************************************************************************/
int main(void)
{
  /* Initialize chip - handle erratas */
  CHIP_Init( );
  /* Initialize clocks and oscillators */
  cmuSetup( );
  /* Initialize UART peripheral */
  uartSetup( );
  /* Initialize Development Kit in EBI mode */
  //BSP_Init(BSP_INIT_DEFAULT);
  /* Enable RS-232 transceiver on Development Kit */
//  BSP_PeripheralAccess(BSP_RS232_UART, true);
  /* When DVK is configured, and no more DVK access is needed, the interface can safely be disabled to save current */
//  BSP_Disable();

  /* Write welcome message to UART */
  uartPutData((uint8_t*) welcomeString, welLen);

  /*  Eternal while loop
   *  CPU will sleep during Rx and Tx. When a byte is transmitted, an interrupt
   *  wakes the CPU which copies the next byte in the txBuf queue to the
   *  UART TXDATA register.
   *
   *  When the predefined termiation character is received, the all pending
   *  data in rxBuf is copied to txBuf and echoed back on the UART */
  while (1)
  {
    /* Wait in EM1 while UART transmits */
    EMU_EnterEM1();
    /* Check if RX buffer has overflowed */
    if (rxBuf.overflow)
    {
      rxBuf.overflow = false;
      uartPutData((uint8_t*) overflowString, ofsLen);
    }
    /* Check if termination character is received */
    if (rxBuf.data[(rxBuf.wrI - 1) % BUFFERSIZE] == TERMINATION_CHAR)
    {
      /* Copy received data to UART transmit queue */
      uint8_t tmpBuf[BUFFERSIZE];
      int     len = uartGetData(tmpBuf, 0);
      uartPutData(tmpBuf, len);
    }

  }

}
/******************************************************************************
* @brief  uartSetup function
*
******************************************************************************/
void uartSetup(void)
{
  /* Enable clock for GPIO module (required for pin configuration) */
  CMU_ClockEnable(cmuClock_GPIO, true);
  /* Configure GPIO pins */
  GPIO_PinModeSet(gpioPortD, 0, gpioModePushPull, 1);
  GPIO_PinModeSet(gpioPortD, 1, gpioModeInput, 0);
  /* Prepare struct for initializing UART in asynchronous mode*/
  uartInit.enable       = usartDisable;   /* Don't enable UART upon intialization */
  uartInit.refFreq      = 0;              /* Provide information on reference frequency. When set to 0, the reference frequency is */
  uartInit.baudrate     = 115200;         /* Baud rate */
  uartInit.oversampling = usartOVS16;     /* Oversampling. Range is 4x, 6x, 8x or 16x */
  uartInit.databits     = usartDatabits8; /* Number of data bits. Range is 4 to 10 */
  uartInit.parity       = usartNoParity;  /* Parity mode */
  uartInit.stopbits     = usartStopbits1; /* Number of stop bits. Range is 0 to 2 */
  uartInit.mvdis        = false;          /* Disable majority voting */
  uartInit.prsRxEnable  = false;          /* Enable USART Rx via Peripheral Reflex System */
  uartInit.prsRxCh      = usartPrsRxCh0;  /* Select PRS channel if enabled */
  /* Initialize USART with uartInit struct */
  USART_InitAsync(uart, &uartInit);
  /* Prepare UART Rx and Tx interrupts */
  USART_IntClear(uart, _UART_IF_MASK);
  USART_IntEnable(uart, UART_IF_RXDATAV);
  NVIC_ClearPendingIRQ(UART1_RX_IRQn);
  NVIC_ClearPendingIRQ(UART1_TX_IRQn);
  NVIC_EnableIRQ(UART1_RX_IRQn);
  NVIC_EnableIRQ(UART1_TX_IRQn);
  /* Enable I/O pins at UART1 location #1 */
  uart->ROUTE = UART_ROUTE_RXPEN | UART_ROUTE_TXPEN | UART_ROUTE_LOCATION_LOC1;
  /* Enable UART */
  USART_Enable(uart, usartEnable);
}
/******************************************************************************
 * @brief  uartGetChar function
 *
 *  Note that if there are no pending characters in the receive buffer, this
 *  function will hang until a character is received.
 *
 *****************************************************************************/
uint8_t uartGetChar( )

{
  uint8_t ch;
  /* Check if there is a byte that is ready to be fetched. If no byte is ready, wait for incoming data */
  if (rxBuf.pendingBytes < 1)
  {
    while (rxBuf.pendingBytes < 1) ;
  }
  /* Copy data from buffer */
  ch        = rxBuf.data[rxBuf.rdI];
  rxBuf.rdI = (rxBuf.rdI + 1) % BUFFERSIZE;

  /* Decrement pending byte counter */
  rxBuf.pendingBytes--;
  return ch;
}
/******************************************************************************
 * @brief  uartPutChar function
 *
 *****************************************************************************/
void uartPutChar(uint8_t ch)
{
  /* Check if Tx queue has room for new data */
  if ((txBuf.pendingBytes + 1) > BUFFERSIZE)
  {
    /* Wait until there is room in queue */
    while ((txBuf.pendingBytes + 1) > BUFFERSIZE) ;
  }
  /* Copy ch into txBuffer */
  txBuf.data[txBuf.wrI] = ch;
  txBuf.wrI             = (txBuf.wrI + 1) % BUFFERSIZE;

  /* Increment pending byte counter */
  txBuf.pendingBytes++;

  /* Enable interrupt on USART TX Buffer*/
  USART_IntEnable(uart, UART_IF_TXBL);
}
/******************************************************************************
 * @brief  uartPutData function
 *
 *****************************************************************************/
void uartPutData(uint8_t * dataPtr, uint32_t dataLen)
{
  uint32_t i = 0;

  /* Check if buffer is large enough for data */
  if (dataLen > BUFFERSIZE)
  {
    /* Buffer can never fit the requested amount of data */
    return;
  }

  /* Check if buffer has room for new data */
  if ((txBuf.pendingBytes + dataLen) > BUFFERSIZE)
  {
    /* Wait until room */
    while ((txBuf.pendingBytes + dataLen) > BUFFERSIZE) ;
  }

  /* Fill dataPtr[0:dataLen-1] into txBuffer */
  while (i < dataLen)
  {
    txBuf.data[txBuf.wrI] = *(dataPtr + i);
    txBuf.wrI             = (txBuf.wrI + 1) % BUFFERSIZE;
    i++;
  }
  /* Increment pending byte counter */
  txBuf.pendingBytes += dataLen;
  /* Enable interrupt on USART TX Buffer*/
  USART_IntEnable(uart, UART_IF_TXBL);
}
/******************************************************************************
 * @brief  uartGetData function
 *
 *****************************************************************************/
uint32_t uartGetData(uint8_t * dataPtr, uint32_t dataLen)
{
  uint32_t i = 0;

  /* Wait until the requested number of bytes are available */
  if (rxBuf.pendingBytes < dataLen)
  {
    while (rxBuf.pendingBytes < dataLen) ;
  }

  if (dataLen == 0)
  {
    dataLen = rxBuf.pendingBytes;
  }

  /* Copy data from Rx buffer to dataPtr */
  while (i < dataLen)
  {
    *(dataPtr + i) = rxBuf.data[rxBuf.rdI];
    rxBuf.rdI      = (rxBuf.rdI + 1) % BUFFERSIZE;
    i++;
  }

  /* Decrement pending byte counter */
  rxBuf.pendingBytes -= dataLen;
  return i;
}
/***************************************************************************//**
 * @brief Set up Clock Management Unit
 ******************************************************************************/
void cmuSetup(void)
{
  /* Start HFXO and wait until it is stable */
  /* CMU_OscillatorEnable( cmuOsc_HFXO, true, true); */

  /* Select HFXO as clock source for HFCLK */
  /* CMU_ClockSelectSet(cmuClock_HF, cmuSelect_HFXO ); */

  /* Disable HFRCO */
  /* CMU_OscillatorEnable( cmuOsc_HFRCO, false, false ); */

  /* Enable clock for HF peripherals */
  CMU_ClockEnable(cmuClock_HFPER, true);

  /* Enable clock for USART module */
  CMU_ClockEnable(cmuClock_UART1, true);
}
/**************************************************************************//**
 * @brief UART1 RX IRQ Handler
 *
 * Set up the interrupt prior to use
 *
 * Note that this function handles overflows in a very simple way.
 *
 *****************************************************************************/
void UART1_RX_IRQHandler(void)
{
  /* Check for RX data valid interrupt */
  if (uart->STATUS & UART_STATUS_RXDATAV)
  {
    /* Copy data into RX Buffer */
    uint8_t rxData = USART_Rx(uart);
    rxBuf.data[rxBuf.wrI] = rxData;
    rxBuf.wrI             = (rxBuf.wrI + 1) % BUFFERSIZE;
    rxBuf.pendingBytes++;

    /* Flag Rx overflow */
    if (rxBuf.pendingBytes > BUFFERSIZE)
    {
      rxBuf.overflow = true;
    }

    /* Clear RXDATAV interrupt */
    USART_IntClear(UART1, UART_IF_RXDATAV);
  }

}
/**************************************************************************//**
 * @brief UART1 TX IRQ Handler
 *
 * Set up the interrupt prior to use
 *
 *****************************************************************************/
void UART1_TX_IRQHandler(void)
{
  /* Check TX buffer level status */
  if (uart->STATUS & UART_STATUS_TXBL)
  {
    if (txBuf.pendingBytes > 0)
    {
      /* Transmit pending character */
      USART_Tx(uart, txBuf.data[txBuf.rdI]);
      txBuf.rdI = (txBuf.rdI + 1) % BUFFERSIZE;
      txBuf.pendingBytes--;
    }

    /* Disable Tx interrupt if no more bytes in queue */
    if (txBuf.pendingBytes == 0)
    {
      USART_IntDisable(uart, UART_IF_TXBL);
    }

  }

}
 

Posts: 556
Registered: ‎05-14-2012

UART using STK3800

Hi

Without looking at your code in detail here, it would be good if you could first check if you actually get any TX signal on your GPIO pin by using a scope or similar. By checking in a terminal program you have many possible other error sources along the way also on the PC side. It is good to start by verifying that you get a basic output at least. 

R


Posts: 28
Registered: ‎08-30-2013

UART using STK3800

Hi,


I have hooked up serail analyzer on the STK3800 (pins 4 and 1) but can not see any data coming out from it. Would the code provided in the Application note 45 work with the STK3800 (minor modifications as stated in my first post)?

Regards


Posts: 28
Registered: ‎08-30-2013

UART using STK3800

Hi,


I have got it working, classic mistake of enabling UART on USART pins! I think I am going to write a quick start guide for the changes that needs to be done in order to use the code for the starter kit (can be helpful to someone else as well).


Regards


Posts: 556
Registered: ‎05-14-2012

UART using STK3800

Hi


Great to hear you got it up and running. There are a few pit falls here, so a quick start guide is very welcome  :-)

R


Posts: 8
Registered: ‎02-17-2014

Re: UART using STK3800

I am on the same situation.

Can you please provide the changes you did to have it on the starter kit without the rs232 device?

Thanks

Posts: 28
Registered: ‎08-30-2013

Re: UART using STK3800

Hi,

Please see the following link for the guide

 

Asynchronous communication using STK3800 Quick Start

 

Regards

Posts: 36
Registered: ‎03-05-2014

Re: UART using STK3800

Hi!

Took your code to test a little bit with my new giant gecko. Problem is, I'm not getting anything out to my Tera Term :-/

Just don't know where the problem is, output pins seem right, tera term also gets signs from other sources. Hope someone could find out where's the problem .....

 

#include "em_device.h"
#include "em_chip.h"
#include "em_cmu.h"
#include "em_gpio.h"
#include "em_emu.h"
#include "em_system.h"
#include "em_usart.h"
//#include "bsp.h"
//#include "bsp_trace.h"

/* Function prototypes */
void uartSetup(void);
void cmuSetup(void);
void uartPutData(uint8_t * dataPtr, uint32_t dataLen);
uint32_t uartGetData(uint8_t * dataPtr, uint32_t dataLen);
void    uartPutChar(uint8_t charPtr);
uint8_t uartGetChar(void);

/* Declare some strings */
const char     welcomeString[]  = "Energy Micro RS-232 - Please press a key";
const char     overflowString[] ="---RX OVERFLOW---";
const uint32_t welLen           = sizeof(welcomeString) - 1;
const uint32_t ofsLen           = sizeof(overflowString) - 1;

/* Define termination character */
#define TERMINATION_CHAR    '.'

/* Declare a circular buffer structure to use for Rx and Tx queues */
#define BUFFERSIZE          256
volatile struct circularBuffer
{
  uint8_t  data[BUFFERSIZE];  /* data buffer */
  uint32_t rdI;               /* read index */
  uint32_t wrI;               /* write index */
  uint32_t pendingBytes;      /* count of how many bytes are not yet handled */
  bool     overflow;          /* buffer overflow indicator */
} rxBuf, txBuf = { {0}, 0, 0, 0, false };

/* Setup UART1 in async mode for RS232*/
static USART_TypeDef           * uart   = UART1;
static USART_InitAsync_TypeDef uartInit = USART_INITASYNC_DEFAULT;
/******************************************************************************
 * @brief  Main function
 *
 *****************************************************************************/
int main(void)
{
  /* Initialize chip - handle erratas */
  CHIP_Init( );
  /* Initialize clocks and oscillators */
  cmuSetup( );
  /* Initialize UART peripheral */
  uartSetup( );
  /* Initialize Development Kit in EBI mode */
  //BSP_Init(BSP_INIT_DEFAULT);
  /* Enable RS-232 transceiver on Development Kit */
//  BSP_PeripheralAccess(BSP_RS232_UART, true);
  /* When DVK is configured, and no more DVK access is needed, the interface can safely be disabled to save current */
//  BSP_Disable();

  /* Write welcome message to UART */
  uartPutData((uint8_t*) welcomeString, welLen);

  /*  Eternal while loop
   *  CPU will sleep during Rx and Tx. When a byte is transmitted, an interrupt
   *  wakes the CPU which copies the next byte in the txBuf queue to the
   *  UART TXDATA register.
   *
   *  When the predefined termiation character is received, the all pending
   *  data in rxBuf is copied to txBuf and echoed back on the UART */
  while (1)
  {
    /* Wait in EM1 while UART transmits */
    EMU_EnterEM1();
    /* Check if RX buffer has overflowed */
    if (rxBuf.overflow)
    {
      rxBuf.overflow = false;
      uartPutData((uint8_t*) overflowString, ofsLen);
    }
    /* Check if termination character is received */
    if (rxBuf.data[(rxBuf.wrI - 1) % BUFFERSIZE] == TERMINATION_CHAR)
    {
      /* Copy received data to UART transmit queue */
      uint8_t tmpBuf[BUFFERSIZE];
      int     len = uartGetData(tmpBuf, 0);
      uartPutData(tmpBuf, len);
    }

  }

}
/******************************************************************************
* @brief  uartSetup function
*
******************************************************************************/
void uartSetup(void)
{
  /* Enable clock for GPIO module (required for pin configuration) */
  CMU_ClockEnable(cmuClock_GPIO, true);
  /* Configure GPIO pins */
  GPIO_PinModeSet(gpioPortD, 0, gpioModePushPull, 1);
  GPIO_PinModeSet(gpioPortD, 1, gpioModeInput, 0);
  /* Prepare struct for initializing UART in asynchronous mode*/
  uartInit.enable       = usartDisable;   /* Don't enable UART upon intialization */
  uartInit.refFreq      = 0;              /* Provide information on reference frequency. When set to 0, the reference frequency is */
  uartInit.baudrate     = 115200;         /* Baud rate */
  uartInit.oversampling = usartOVS16;     /* Oversampling. Range is 4x, 6x, 8x or 16x */
  uartInit.databits     = usartDatabits8; /* Number of data bits. Range is 4 to 10 */
  uartInit.parity       = usartNoParity;  /* Parity mode */
  uartInit.stopbits     = usartStopbits1; /* Number of stop bits. Range is 0 to 2 */
  uartInit.mvdis        = false;          /* Disable majority voting */
  uartInit.prsRxEnable  = false;          /* Enable USART Rx via Peripheral Reflex System */
  uartInit.prsRxCh      = usartPrsRxCh0;  /* Select PRS channel if enabled */
  /* Initialize USART with uartInit struct */
  USART_InitAsync(uart, &uartInit);
  /* Prepare UART Rx and Tx interrupts */
  USART_IntClear(uart, _UART_IF_MASK);
  USART_IntEnable(uart, UART_IF_RXDATAV);
  NVIC_ClearPendingIRQ(UART1_RX_IRQn);
  NVIC_ClearPendingIRQ(UART1_TX_IRQn);
  NVIC_EnableIRQ(UART1_RX_IRQn);
  NVIC_EnableIRQ(UART1_TX_IRQn);
  /* Enable I/O pins at UART1 location #1 */
  uart->ROUTE = UART_ROUTE_RXPEN | UART_ROUTE_TXPEN | UART_ROUTE_LOCATION_LOC1;
  /* Enable UART */
  USART_Enable(uart, usartEnable);
}
/******************************************************************************
 * @brief  uartGetChar function
 *
 *  Note that if there are no pending characters in the receive buffer, this
 *  function will hang until a character is received.
 *
 *****************************************************************************/
uint8_t uartGetChar( )

{
  uint8_t ch;
  /* Check if there is a byte that is ready to be fetched. If no byte is ready, wait for incoming data */
  if (rxBuf.pendingBytes < 1)
  {
    while (rxBuf.pendingBytes < 1) ;
  }
  /* Copy data from buffer */
  ch        = rxBuf.data[rxBuf.rdI];
  rxBuf.rdI = (rxBuf.rdI + 1) % BUFFERSIZE;

  /* Decrement pending byte counter */
  rxBuf.pendingBytes--;
  return ch;
}
/******************************************************************************
 * @brief  uartPutChar function
 *
 *****************************************************************************/
void uartPutChar(uint8_t ch)
{
  /* Check if Tx queue has room for new data */
  if ((txBuf.pendingBytes + 1) > BUFFERSIZE)
  {
    /* Wait until there is room in queue */
    while ((txBuf.pendingBytes + 1) > BUFFERSIZE) ;
  }
  /* Copy ch into txBuffer */
  txBuf.data[txBuf.wrI] = ch;
  txBuf.wrI             = (txBuf.wrI + 1) % BUFFERSIZE;

  /* Increment pending byte counter */
  txBuf.pendingBytes++;

  /* Enable interrupt on USART TX Buffer*/
  USART_IntEnable(uart, UART_IF_TXBL);
}
/******************************************************************************
 * @brief  uartPutData function
 *
 *****************************************************************************/
void uartPutData(uint8_t * dataPtr, uint32_t dataLen)
{
  uint32_t i = 0;

  /* Check if buffer is large enough for data */
  if (dataLen > BUFFERSIZE)
  {
    /* Buffer can never fit the requested amount of data */
    return;
  }

  /* Check if buffer has room for new data */
  if ((txBuf.pendingBytes + dataLen) > BUFFERSIZE)
  {
    /* Wait until room */
    while ((txBuf.pendingBytes + dataLen) > BUFFERSIZE) ;
  }

  /* Fill dataPtr[0:dataLen-1] into txBuffer */
  while (i < dataLen)
  {
    txBuf.data[txBuf.wrI] = *(dataPtr + i);
    txBuf.wrI             = (txBuf.wrI + 1) % BUFFERSIZE;
    i++;
  }
  /* Increment pending byte counter */
  txBuf.pendingBytes += dataLen;
  /* Enable interrupt on USART TX Buffer*/
  USART_IntEnable(uart, UART_IF_TXBL);
}
/******************************************************************************
 * @brief  uartGetData function
 *
 *****************************************************************************/
uint32_t uartGetData(uint8_t * dataPtr, uint32_t dataLen)
{
  uint32_t i = 0;

  /* Wait until the requested number of bytes are available */
  if (rxBuf.pendingBytes < dataLen)
  {
    while (rxBuf.pendingBytes < dataLen) ;
  }

  if (dataLen == 0)
  {
    dataLen = rxBuf.pendingBytes;
  }

  /* Copy data from Rx buffer to dataPtr */
  while (i < dataLen)
  {
    *(dataPtr + i) = rxBuf.data[rxBuf.rdI];
    rxBuf.rdI      = (rxBuf.rdI + 1) % BUFFERSIZE;
    i++;
  }

  /* Decrement pending byte counter */
  rxBuf.pendingBytes -= dataLen;
  return i;
}
/***************************************************************************//**
 * @brief Set up Clock Management Unit
 ******************************************************************************/
void cmuSetup(void)
{
  /* Start HFXO and wait until it is stable */
  /* CMU_OscillatorEnable( cmuOsc_HFXO, true, true); */

  /* Select HFXO as clock source for HFCLK */
  /* CMU_ClockSelectSet(cmuClock_HF, cmuSelect_HFXO ); */

  /* Disable HFRCO */
  /* CMU_OscillatorEnable( cmuOsc_HFRCO, false, false ); */

  /* Enable clock for HF peripherals */
  CMU_ClockEnable(cmuClock_HFPER, true);

  /* Enable clock for USART module */
  CMU_ClockEnable(cmuClock_UART1, true);
}
/**************************************************************************//**
 * @brief UART1 RX IRQ Handler
 *
 * Set up the interrupt prior to use
 *
 * Note that this function handles overflows in a very simple way.
 *
 *****************************************************************************/
void UART1_RX_IRQHandler(void)
{
  /* Check for RX data valid interrupt */
  if (uart->STATUS & UART_STATUS_RXDATAV)
  {
    /* Copy data into RX Buffer */
    uint8_t rxData = USART_Rx(uart);
    rxBuf.data[rxBuf.wrI] = rxData;
    rxBuf.wrI             = (rxBuf.wrI + 1) % BUFFERSIZE;
    rxBuf.pendingBytes++;

    /* Flag Rx overflow */
    if (rxBuf.pendingBytes > BUFFERSIZE)
    {
      rxBuf.overflow = true;
    }

    /* Clear RXDATAV interrupt */
    USART_IntClear(UART1, UART_IF_RXDATAV);
  }

}
/**************************************************************************//**
 * @brief UART1 TX IRQ Handler
 *
 * Set up the interrupt prior to use
 *
 *****************************************************************************/
void UART1_TX_IRQHandler(void)
{
  /* Check TX buffer level status */
  if (uart->STATUS & UART_STATUS_TXBL)
  {
    if (txBuf.pendingBytes > 0)
    {
      /* Transmit pending character */
      USART_Tx(uart, txBuf.data[txBuf.rdI]);
      txBuf.rdI = (txBuf.rdI + 1) % BUFFERSIZE;
      txBuf.pendingBytes--;
    }

    /* Disable Tx interrupt if no more bytes in queue */
    if (txBuf.pendingBytes == 0)
    {
      USART_IntDisable(uart, UART_IF_TXBL);
    }

  }

}

 

Posts: 28
Registered: ‎08-30-2013

Re: UART using STK3800

Hi,

 

A quick glance at the code tells me that you are trying to configure UART1 where as you are using USART1 pins, please confirm the pins and if this is the case then you need to replace UART1 name with USART1.

 

Please see the link below for detailed explanation:

 

Asynchronous communication using STK3800 Quick Start

 

Regards

Posts: 6
Registered: ‎05-25-2014

Re: UART using STK3800

[ Edited ]

Are you able to raise and if you have to give the code had it fixed?

Posts: 15
Registered: ‎01-05-2015

Re: UART using STK3800

The sample works when everything gets renamed to USART1.

 

One question, where have you found this sample code, in my Wonder examples it is not included.

 

Regards Helmut

<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero Employee</font></font> </a> Alf
Posts: 280
Registered: ‎09-06-2012

Re: UART using STK3800

Hi,

 

All the examples come with Simplicity Studio. You can download it for free here: http://www.silabs.com/products/mcu/Pages/simplicity-studio-getting-started.aspx

 

If you already have Simplicity Studio v3, make sure to add the Wonder Gecko components to get the examples.

 

My views are my own and do not necessarily represent the views of Silicon Labs
Posts: 15
Registered: ‎01-05-2015

Re: UART using STK3800

Hi Alf, I have v3 installed, Wonder selected and searched in every of the 30 "Example Codes", I have not seen this code. Is this is located in a directory which is not selectable within the IDE?, Where?

 

Regards Helmut