Reply
Posts: 22
Registered: ‎02-16-2015

The New Giant Gecko Series 1 is Here!

Hi everyone,

 

We have just launched our next-generation version of the Giant Gecko MCU, the EFM32GG11. It follows in the footsteps of the original Giant Gecko, by providing a wide range of functionality and high level of performance in a small and extremely energy efficient package. It brings new functionality such as CAN, SDIO, Quad-SPI and Ethernet to the family, as well as all the functionality of the original Giant Gecko, including Segment LCD, backup mode, USB and TFT controller. The MCU has up to 2 MB flash and 512 kB RAM, and runs up to 72 MHz, with current consumption as low as 77 uA/MHz and 1.6 uA in EM2.

 

The Micrium OS kernel will be provided for free to help jumpstart projects on the EFM32GG11.  Flexible paid license options are available for advanced drivers and stacks such as Ethernet and SDIO, providing a robust production-ready solution.

 

Note that this is an ‘Engineering Status’ launch. Kits and limited numbers of ICs will be available starting today, with production scheduled to start in Q1 of 2018.

 

To learn more about the new EFM32 Giant Gecko Series 1, check out the links below:

https://www.silabs.com/products/mcu/32-bit/efm32-giant-gecko-gg11

http://news.silabs.com/2017-07-24-Feature-Rich-Giant-Gecko-Microcontrollers-Help-Developers-Tackle-C...

 

-Øivind

Posts: 5
Registered: ‎10-12-2015

Re: The New Giant Gecko Series 1 is Here!

Looks great!

 

Hoping you get a move on filling out the Series 1 range myself! This one helps a lot but its also no more than a couple more very rough grained configuration options for now. The series is begging for more memory/package/price configurations. We are engineers dammit. Must... optimize... mcu... selection Robot Mad

Posts: 123
Registered: ‎10-01-2012

Re: The New Giant Gecko Series 1 is Here!

Very cool!

 

Regarding "SD/SDIO" peripheral, does this mean eMMC devices (which drop support for the SD SPI mode) are now supported in hardware?

Posts: 582
Registered: ‎09-18-2015

Re: The New Giant Gecko Series 1 is Here!

Hi @Drmn4ea,

 

Regarding "SD/SDIO" peripheral, does this mean eMMC devices (which drop support for the SD SPI mode) are now supported in hardware?

 

Yes!

 

John

Posts: 123
Registered: ‎09-15-2013

Re: The New Giant Gecko Series 1 is Here!

Finallyyy...

Posts: 32
Registered: ‎10-08-2013

Re: The New Giant Gecko Series 1 is Here!

Are there any Ethernet software samples? Could not find them in SDK.

Posts: 22
Registered: ‎02-16-2015

Re: The New Giant Gecko Series 1 is Here!

Hi @Slowmo


Slowmo wrote:

Are there any Ethernet software samples? Could not find them in SDK.


There is one Ethernet example available at this point. Check out the 'SLSTK3701A_micriumos_net' demo

 

-Oivind

Posts: 22
Registered: ‎02-16-2015

Re: The New Giant Gecko Series 1 is Here!

Hi @Joku,

 

We are working on it. Anything specific you are looking for?

 

-Øivind

Posts: 32
Registered: ‎10-08-2013

Re: The New Giant Gecko Series 1 is Here!


There is one Ethernet example available at this point. Check out the 'SLSTK3701A_micriumos_net' demo
 

So Ethernet is meant to be used in Micrium OS, right? Will there be a software stack to enable Ethernet in regular projects without an OS?

Posts: 22
Registered: ‎02-16-2015

Re: The New Giant Gecko Series 1 is Here!


So Ethernet is meant to be used in Micrium OS, right? Will there be a software stack to enable Ethernet in regular projects without an OS?


Software support for Ethernet is currently only provided through Micrium OS. There are multiple reasons for this: By providing it with Micrium OS we can make sure the Ethernet stack will work well with the rest of the system, even if the rest of the system is complex and uses multiple other peripherals, such as USB or SDIO. This ultimately makes it easier to build a robust application which will not fail in the field under load or when hit with special situations.

 

We also believe most applications built on the EFM32GG11 will be based on an RTOS, in order to help manage complexity

Posts: 1
Registered: ‎08-04-2017

Re: The New Giant Gecko Series 1 is Here!

Hi Oivind_L,

    The supported Ethernet provided through Micrium OS is also free?

     There's plans to support LwIP with Micrium OS?

      The Micrium OS kernel will be free as source code or only as lib?

 

      Ari. 

Posts: 32
Registered: ‎10-08-2013

Re: The New Giant Gecko Series 1 is Here!

Good point. If Ethernet is only usable through Micrium, I would expect TCP/IP stack to be free as well, otherwise we can not use part of the hardware inside the new MCU.

Posts: 5
Registered: ‎10-12-2015

Re: The New Giant Gecko Series 1 is Here!

Hi @Oivind_L

 

I appreciate that your priority with Series 1 is going to be towards solutions that have less overlap with Series 0, and that I can't expect too much from a relatively new series. But for those of us who want minor features that only exist on Series 1, the range looks awfully rough at this stage.

 

My major issues are these:

 

- Lack of any mid or low price point solutions in a non BGA package above 48 pins at this point. I think the limited package options make a lot less sense on Pearl/Jade than they do on the equivalent EFR SoC's when you consider the external RF transceiver case and Pearl/Jade's NC pins. I think QFN64 is sorely missed on Pearl/Jade, and if that isn't going to come then I guess what I'm hoping for is that this new GG11 series gets variants with some of the high end peripherals cut out and number of low end peripherals reduced along with significantly reduced memory configurations, so the low end QFN64 variant reaches a fair way down into the mid range price bracket. 

 

- Lack of a budget oriented alternative to xG1 given that xG1 carries unique issues. The xG13 or the half-RAM xG12 that both exist in the SoC range would go a significant way to resolving this.

Posts: 22
Registered: ‎02-16-2015

Re: The New Giant Gecko Series 1 is Here!

Hi @Joku,

 

Your requests make sense. We are in fact working on broadening the offering as we speak. Look for more information towards the end of the year. Note that the additions we will be making will be very compatible with the GG11 we just launched, so GG11 is a very good starting point.

 

-Øivind

Posts: 22
Registered: ‎02-16-2015

Re: The New Giant Gecko Series 1 is Here!


Slowmo wrote:

Good point. If Ethernet is only usable through Micrium, I would expect TCP/IP stack to be free as well, otherwise we can not use part of the hardware inside the new MCU.


Can you explain your use-case to me? Are you looking at using the this for a commercial product where you need Ethernet, TCP/IP etc?

Posts: 22
Registered: ‎02-16-2015

Re: The New Giant Gecko Series 1 is Here!

Hi @amsantos,

 

The Network stack provided through Micrium OS is not free. In order to provide the level of quality and support that is required for it, it does come at a cost. There are currently no plans to support LwIP on Micrium OS. The hardware would be capable of it, but we have decided to focus our efforts on delivering one good solution vs delivering multiple half-baked solutions. 

 

The Micrium OS Kernel is provided as source, and is free to use for Silicon Labs MCUs and Wireless MCUs.

 

-Øivind

Posts: 2
Registered: ‎10-22-2016

Re: The New Giant Gecko Series 1 is Here!

@Oivind_L,

 

So there is no option to get Ethernet running without stack that needs a license. Then where can I find all the prices for licensed stacks (at least modbus and ethernet)? I'm curious how it will compete with ST and freeRTOS..

Why there is almost no information about all the licenses and policy how they are applied? 

Posts: 32
Registered: ‎10-08-2013

Re: The New Giant Gecko Series 1 is Here!

Oivind_L wrote:

Slowmo wrote:

Good point. If Ethernet is only usable through Micrium, I would expect TCP/IP stack to be free as well, otherwise we can not use part of the hardware inside the new MCU.


Can you explain your use-case to me? Are you looking at using the this for a commercial product where you need Ethernet, TCP/IP etc?


Yes, it is intended as a commercial product, which collects data from large sensor network and sends it to remote server using REST calls. Built in web server would also be necessary to allow for status monitoring and configuration.

We now have to decide on the chipset to use, and GG11 in conjunction with Micrium OS seems just what we need apart from it being an EFM part not EZR. We could use a Sub-Ghz radio in the same package as well. But given, that there is not much information on pricing of Micrium stacks and modules, it is hard to make GG11 as our first choice right now.

Posts: 22
Registered: ‎02-16-2015

Re: The New Giant Gecko Series 1 is Here!

@Slowmo and @agl123,

 

Prices for these types of components are typically not published online, because they depend on what you need, and the use-case. I would suggest you talk with your Silicon Labs sales rep, or go to the following link to get more information on pricing: https://www.silabs.com/buysample/pages/contact-sales.aspx

 

 

Posts: 22
Registered: ‎02-16-2015

Re: The New Giant Gecko Series 1 is Here!

@Slowmo and @agl123,

 

Another option to discuss Micrium pricing is to send an email to sales@micrium.com or call +1 512 464 9401

 

-Øivind

Posts: 3
Registered: ‎08-09-2017

Re: The New Giant Gecko Series 1 is Here!

Hi,

 

I got the new EFM32GG11 Starter Kit. When I try to use the Hardware Configurator I get an NullPointerException and I cannot configure the device. Is the Starter Kit included in the SDK?

Posts: 22
Registered: ‎02-16-2015

Re: The New Giant Gecko Series 1 is Here!

Hi @VerenaP,

 

The HW Configurator does not yet support the GG11. It is planned for Q4 of this year. You should still not get a null pointer exception though. Can you submit a bug report for that?

 

-Øivind

Posts: 28
Registered: ‎04-07-2017

Re: The New Giant Gecko Series 1 is Here!

We are trying to evaluate the EFM32GG11 Starter Kit. I recently updated Simplicity Studio, but I didn't see any software example projects for the board. When will you have examples? I'm particularly interested in the FreeRTOS example

 

Thank you.

Posts: 1
Registered: ‎09-01-2017

Re: The New Giant Gecko Series 1 is Here!

Hi,

 

One of our board is using a Cortex-M3 EFM32GG990F1024. Do the new EFM32GG11 pins be the same? We are using a BGA112 package.

 

Thank you.

Posts: 2,384
Registered: ‎10-14-2014

Re: The New Giant Gecko Series 1 is Here!

I don't think GG11 would pin compatible with GG990F1024 (BGA112). GG11 datasheet only cover BGA192 and BGA100, though there are other package option acocring this page.

And the peripheral route strategy for GG11 was changed a lot. The peripheral type supported changes a lot also.

 

Even for same QFP100 package, you could see the difference in the pinout section of the datasheet.

https://www.silabs.com/documents/public/data-sheets/EFM32GG380.pdf

https://www.silabs.com/documents/public/data-sheets/efm32gg11-datasheet.pdf

 

My views are my own and do not necessarily represent the views of Silicon Labs

 

 

WeiguoLu
Posts: 22
Registered: ‎02-16-2015

Re: The New Giant Gecko Series 1 is Here!

Hi @Ivanoway,

 

Many more package options are coming for the GG11, including QFP64, QFN64, BGA120 and BGA152, including multiple that will be pin-compatible with the existing Giant Gecko. EFM32GG990F1024 will have a pin-compatible package. These additional packages will become available as we go into full production early next year.

 

-Øivind

Posts: 22
Registered: ‎02-16-2015

Re: The New Giant Gecko Series 1 is Here!

Hi @richdinoso,

 

Demos are available in Simplicity Studio. Make sure you have updated Studio if you are using an existing installation, and that you have selected the latest SDK. There are currently no FreeRTOS examples in the SDK for the GG11, but there are a number of MicriumOS examples, stretching from blinky to USB and Ethernet.

 

Hope this helps! Let us know if you still have trouble getting it working

-Øivind

Posts: 28
Registered: ‎04-07-2017

Re: The New Giant Gecko Series 1 is Here!

Hello @Oivind_L,

 

Thank you for the reply. We are more interested in FreeRTOS instead of MicriumOS because of the cost factor. Are there plans to provide FreeRTOS examples in Simplicity Studio in the near future?

 

Thank you.

Posts: 1
Registered: ‎09-13-2017

Re: The New Giant Gecko Series 1 is Here!

Awesome! This is one of the best i've seen from Silicon Labs yet. 

Posts: 2
Registered: ‎09-28-2017

Re: The New Giant Gecko Series 1 is Here!

Hello,

plz, I can not compile SLSTK3701A_micriumos_net for AFM32GG11

the folder /net is empty

logs

arm-none-eabi-gcc -g -gdwarf-2 -mcpu=cortex-m4 -mthumb -std=c99 '-DDEBUG_EFM=1' '-DRETARGET_VCOM=1' '-DEFM32GG11B820F2048GL192=1' '-DDEBUG=1' -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//app/mcu_example/SLSTK3701A_EFM32GG11/micriumos_net/net/core" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//app/mcu_example/SLSTK3701A_EFM32GG11/micriumos_net/net" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//app/mcu_example/SLSTK3701A_EFM32GG11/micriumos_net/common/common" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//util/micrium/Micrium_OS/rtos/net/source/dns" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//util/micrium/Micrium_OS/rtos/net/source/dhcp" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//util/micrium/Micrium_OS/rtos/net/source/util" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//util/micrium/Micrium_OS/rtos/net/source/tcpip" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//util/micrium/Micrium_OS/rtos/kernel/source/ports/armv7-m/gnu" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//util/micrium/Micrium_OS/rtos/kernel/source/ports/armv7-m/iar" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//util/micrium/Micrium_OS/rtos/kernel/source" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//util/micrium/Micrium_OS/rtos/drivers/net/source" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//util/micrium/Micrium_OS/rtos/cpu/source/ports/interrupt/armv7-m" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//util/micrium/Micrium_OS/rtos/cpu/source/ports/armv7-m/gnu" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//util/micrium/Micrium_OS/rtos/cpu/source/ports/armv7-m/iar" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//util/micrium/Micrium_OS/rtos/cpu/source" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//util/micrium/Micrium_OS/rtos/common/source/platform_mgr" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//util/micrium/Micrium_OS/rtos/common/source/rtos" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//util/micrium/Micrium_OS/rtos/common/source/lib" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//util/micrium/Micrium_OS/rtos/common/source/kal" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//util/micrium/Micrium_OS/rtos/common/source/common" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//util/micrium/Micrium_OS/rtos/common/source/collections" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//util/micrium/Micrium_OS/rtos/common/source/clk" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//util/micrium/Micrium_OS/rtos/common/source/auth" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//util/micrium/Micrium_OS/bsp/siliconlabs/generic/source" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//util/micrium/Ports/CMSIS/IAR" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//util/micrium/Ports/CMSIS/GCC" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//util/micrium/Micrium_OS" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//util/micrium/Micrium_OS/bsp/siliconlabs/generic/include" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//app/mcu_example/SLSTK3701A_EFM32GG11/micriumos_net/cfg" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//app/mcu_example/SLSTK3701A_EFM32GG11/micriumos_net" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//hardware/kit/SLSTK3701A_EFM32GG11/config" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//platform/CMSIS/Include" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//platform/emlib/inc" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//hardware/kit/common/bsp" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//hardware/kit/common/drivers" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//platform/Device/SiliconLabs/EFM32GG11B/Include" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//platform/middleware/glib" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//platform/middleware/glib/glib" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//platform/middleware/glib/dmd" -I"C:/SiliconLabs/SimplicityStudio/v4/developer/sdks/gecko_sdk_suite/v1.1//platform/middleware/glib/dmd/ssd2119" -O0 -Wall -c -fmessage-length=0 -mno-sched-prolog -fno-builtin -ffunction-sections -fdata-sections -mfpu=fpv4-sp-d16 -mfloat-abi=softfp -MMD -MP -MF"src/graphics.d" -MT"src/graphics.o" -o "src/graphics.o" "../src/graphics.c"
Finished building: ../src/ex_common_init.c
make: *** [src/ex_net_core.o] Error 1
make: *** Waiting for unfinished jobs....

Finished building: ../src/ex_main.c
Finished building: ../src/ex_network.c


../src/graphics.c:20:37: fatal error: rtos/net/include/net_if.h: No such file or directory
#include <rtos/net/include/net_if.h>
^
compilation terminated.
make: *** [src/graphics.o] Error 1

 

Posts: 2
Registered: ‎09-28-2017

Re: The New Giant Gecko Series 1 is Here!

Hello,

plz, I can not compile  SLSTK3701A_micriumos_net

after checkout the net folder is empty

in includes ../Micrium_OS/rtos/net/source/tcpip does not exist

and in compilation the net.h file can not be found : see attach

Posts: 439
Registered: ‎07-13-2015

Re: The New Giant Gecko Series 1 is Here!

Hi,

 

I'd be very excited to try the new Giant Gecko, but where is the QFN64 version?

The product website says it is available in QFN64, but then the devices list does not contain any actual device with QFN64. What's going on?

Posts: 23
Registered: ‎11-11-2015

Re: The New Giant Gecko Series 1 is Here!

Hi Timur,

 

currently only BGA192 and TQFP100 packages are shipping. Per Oivind's answer above, other package options (including QFN64) will become available early next year.

Posts: 439
Registered: ‎07-13-2015

Re: The New Giant Gecko Series 1 is Here!

Do I see it correctly that you guys are trying to create a vendor lock-in for your microcontrollers with Micrium OS and Simplicity Studio? At least the fact that you can only use the Ethernet from Micrium OS is very worrying. (Just like the fact that the EFR was not usable with GCC in the beginning.) This is exactly why I disliked TI: their hardware is locked to their software stack.

 

I preferred Silicon Labs products because I was free to use whatever piece of software I like, and am free to write my own. (Except for the undocumented radio of the EFR, of course.)

 

For TI (in my opinion) this approach resulted in a general loss of quality: because they were only meant to be used with their software stack, many MCU peripherals and drivers are now poorly documented and poorly tested. Of course their software stack only works with their own compiler, which is so hard-to-use that you can only use it with their build tools and their IDE. But then their IDE (yet another Eclipse rip-off, just like Simplicity Studio) is a mess: it's slow, quirky and frustrating.

 

Please don't go in the same direction.

Posts: 123
Registered: ‎10-01-2012

Re: The New Giant Gecko Series 1 is Here!

@Timur Agreed. I was even willing to maintain blissful ignorance when talking about complete network (software) stacks over the peripheral, but in this thread Silabs made it clear that basic hardware peripherals like 4-bit SD/MMC won't even get so much as emlib headers; they will only be supported via Micrium (or maybe raw register-banging on your own hands and knees). A followup question about what other HW peripherals this policy would apply to remains unanswered.

Posts: 439
Registered: ‎07-13-2015

Re: The New Giant Gecko Series 1 is Here!

@Drmn4eaWhoah, so it's not only ethernet but also the SD/MMC? So basically the hardware is entirely useless if I don't wanna buy into their OS?

Posts: 22
Registered: ‎02-16-2015

Re: The New Giant Gecko Series 1 is Here!

Hi @Timur and @Drmn4ea,

 

For the EFM32 MCUs, including EFM32GG11, you can easily use other IDEs such as IAR if you prefer that. Simplicity Studio provides a convenient package of tools, demos etc, and will work side-by-side IAR if you want access to those, or you can use an IDE such as IAR stand-alone. It is up to you.

 

All the EFM32 peripherals are documented in the reference manual: https://www.silabs.com/documents/public/reference-manuals/efm32gg11-rm.pdf, and you will also find CMSIS headers for all peripherals. This also includes SDIO and Ethernet.

 

You are right that we have made some priority calls on what software stacks to provide for the EFM32GG11, in order to maximize ease of use of complex peripherals such as SDIO and Ethernet. The documentation and headers for these peripherals are available, so if you want to port an existing driver, that is always possible.

 

Best Regards

-Øivind

Posts: 439
Registered: ‎07-13-2015

Re: The New Giant Gecko Series 1 is Here!

Thank you @Oivind_L for the clarification!

 

About IDE choice: No, I don't prefer IAR either (it costs a fortune and is out of scope for us), and Simplicity Studio is too slow and crashes often. I presently just use Qt Creator together with the JLink software which is much less painful.

 

SDIO and ETH: nice to see that at least the hardware is well-documented (unlike the EFR radio, which is still a bad trend), but I would have welcomed an emdrv driver for them as well. Maybe Silicon Labs could eventually implement that too?

Posts: 22
Registered: ‎02-16-2015

Re: The New Giant Gecko Series 1 is Here!

Hi @Timur,

 

You are welcome!

 

>SDIO and ETH: nice to see that at least the hardware is well-documented (unlike the EFR radio, which is still a bad trend), but I would have welcomed an emdrv driver for them as well. Maybe Silicon Labs could eventually implement that too?

 

There will likely not be an emdrv driver for these. I think most people using Ethernet will want to use Eth with a full IP stack, which complicates the picture. Similarly for SDIO, you want to use that either with a file-system or an IP stack depending on your use-case. This is why we are going the MicriumOS route for these, as we can more easily provide the complete functionality. A solution in emdrv would require developers to put the pieces together themselves, which could be fun, but would take much more development time.

 

> well-documented (unlike the EFR radio, which is still a bad trend)


There are some good reasons for this. By not documenting the internals, and rather focusing developers on e.g. the RAIL API, we can put more innovation into the hardware, improving it and changing architectures etc. without breaking application code. 

 

-Øivind

 

 

 

 

Posts: 582
Registered: ‎09-18-2015

Re: The New Giant Gecko Series 1 is Here!

Hi @Timur,

 

Having read our internal documentation for the radio controller, I feel that our means of delivering access to the radio via our software abstraction layer is the way to go.

 

While I agree it would be nice to have full documentation — perhaps for the purpose of developing an open source radio driver — the fact of the matter is that few engineers have a thorough understanding of software-defined radio, a term that has been around since I started at Motorola SPS back in the 1990's but is absolutely reality now in the way that we deliver it on our EFR32 devices.

 

That so few engineers outside the realm of our specific role as a device manufacturer have this expertise speaks to the absolute chaos that might ensue were we to make this interface wide open Smiley Surprised It is challenging enough to support the digital and analog sides of these devices as we integrate more and more features. Opening up the RF side of the house probably generates little goodwill for us despite the out-sized effort involved.

 

In this respect, our RAIL (Radio Abstraction Interface Layer) really does give you a very complete API with which to access and control the software end of the radio without delving into things like how the underlying hardware guts work (think state machine, associated data management logic, etc).

 

Under the circumstances, this lets us deliver what matters most: protocol stacks that are compliant with the latest standards (BLE, Thread, ZigBee, and such) as well as letting customers develop fully-customized software-defined radio implementations for proprietary and legacy standards (e.g. wireless X-10).

 

Anyway, these are just the opinions of someone who answers your questions daily about how to use our devices and who understands the value of full hardware documentation, having most recently spent a stint at a chip company very heavily dependent on open source software that otherwise left much of their core hardware undocumented and reliant on binary-only Linux drivers (think GPUs and VPUs).

 

John

Posts: 3,153
Registered: ‎02-07-2002

Re: The New Giant Gecko Series 1 is Here!

But not opening up RAIL c.s. also means that we cannot find the bugs that you put in there (see RAIL-short-SYNC-word). Or to find out what you really meant by the poor documentation (see RAIL-address-filtering).