Reply
Posts: 5
Registered: ‎08-09-2016
Accepted Solution

Simplicity studio SDK5.2.2.0 - STK3700 biometric demo not working

I've a fresh install of Simplicity Studio with SDK 5.2.2.0, but trying to run STK3700 biometric demo, I always get error on uint16_t that could not be resolved. I recall it was working well with SDK 4.4.1, is there any further setting to do due to different SDK?

 

Thanks for any advice.

Posts: 2,386
Registered: ‎10-14-2014

Re: Simplicity studio SDK5.2.2.0 - STK3700 biometric demo not working

Do you mind uploading a screenshot (or compiling log file) to show the issue.

I tried this project and did not found the issue on my side.

WeiguoLu
Posts: 5
Registered: ‎08-09-2016

Re: Simplicity studio SDK5.2.2.0 - STK3700 biometric demo not working

WeiguoLu,

thanks for you reply. Actually this morning after some updates, biometric demo is able to build without errors. Yet I'm not clear what happened and basically I've the same problem with an old project that was running with sdk 4.4.1. I will dig more into the problem and let you know.

 

Thanks,

Posts: 5
Registered: ‎08-09-2016

Re: Simplicity studio SDK5.2.2.0 - STK3700 biometric demo not working

Hi WeiguoLu,

FYI I've tried to import AN0042 EFM32 bootloader project, but I got the error message:

Unable to download asset://efm32/appnote/an0042_efm32_usb_uart_bootloader/an0042-efm32-usb-uart-bootloader.pdf
Failed to download https://devtools.silabs.com/studio/v4/assets//efm32/appnote/an0042_efm32_usb_uart_bootloader.zip.tim...

 

On other hand, Software examples are loaded and imported correctly by Simplicity Studio as well as I'm able to login with my credential.

 

Any advise how to solve this?

 

Thanks,