Reply
Posts: 8
Registered: ‎02-07-2014

Olimex dev board

Hi all,

 

I want to buy dev board from Olimex: EM-32G210F128-H

 

I have one board from STM, STM32L-DISCOVERY whic have on board

ST-Link/V2 for programming and debugging in SWD mode.

Can I use this programmer for programming Olimex  EM-32G210F128-H board?

 

regards

 

Eggy

 

 

Posts: 7,951
Registered: ‎08-13-2003

Re: Olimex dev board

Olimex, STM

 

what does that have to do in a Silicon Labs forum?

erik
Posts: 8
Registered: ‎02-07-2014

Re: Olimex dev board

This Olimex board is based on EFM32G210F128.

But I don't have money for another programmer/debugger

so my question is, can I use this programmer/debugger from

STM board which supports SWD? 

 

Posts: 267
Registered: ‎03-14-2014

Re: Olimex dev board

The olimax docs are up to there normal very low standard! So I dont know, but it's unlikely, having said that, give it a go.

You would have been better spending slightly more and getting a STK (starter kit) from here. All the EFM STK's can program any of the EFM chip's, even ones on boards you make yourself and kits like olimax.

I have a feeling the ST board wont work, but nothing to loose by trying. The REAL GECKO boards are much better, I have some Olimax stuff and I am not impressed with it

LG

Posts: 47
Registered: ‎10-10-2012

Re: Olimex dev board

Hi Eggy

 

May be it is possible to use your ST-Link/V2 with your Olimex EM-32G210F128-H Board over Openocd:

 

http://sourceforge.net/p/openocd/mailman/openocd-user/thread/5330AF5C.2000005@op.pl/

 

Posts: 47
Registered: ‎10-10-2012

Re: Olimex dev board

I tested OpenOCD with the EM-32G880F128-STK Board and STM32F4Discovery Board and I was able to reset and halt the device and read out some registers.

 

I collect my results and information here:

https://github.com/nopeppermint/openocd_efm32

 

Maybe someone have an idea how to flash with OpenOCD, at the moment I'm trying to do this...

 

Regards Stefan

Highlighted
Posts: 47
Registered: ‎10-10-2012

Re: Olimex dev board

[ Edited ]

I'm now able to flash an EFM32 uC on the EM-32G880F128-STK Board with the ST-LINK/V2 on the STM32F4Discovery Board over OpenOCD.

 

@eggy 

I have no EM-32G210F128-H Board at the moment, but the bin file here

https://github.com/nopeppermint/Olimex_EFM32_CoLinkEx_Example/tree/master/00_Blinky_Keil_EM-32G10F12...

should work, I tested It last year on the olimex board.