Reply
Highlighted
Posts: 7
Registered: ‎05-27-2013

New EFM32 Pearl and Jade Gecko devices launched!

Hi everyone,


I'm excited to announce that two new members of the Pearl and Jade Gecko families launched today -  PG12 and JG12:

 

http://news.silabs.com/press-release/corporate-news/gecko-microcontrollers-get-big-boost-security-me...

 

These new devices extend Pearl and Jade Gecko to 1MB flash, 256KB RAM, and add new on-chip peripheral and security features.  Learn more about them here:

http://www.silabs.com/pearlgecko
http://www.silabs.com/jadegecko

 

Regards,

Ted

Posts: 53
Registered: ‎01-04-2010

Re: New EFM32 Pearl and Jade Gecko devices launched!

Hello,

JG12 and PG12 looks very interesting for me.

Order samples, prepare PCB and now wait...

May be you increase samples amount from 2 to 5 ?

 

Thanks !

 

Posts: 7
Registered: ‎05-27-2013

Re: New EFM32 Pearl and Jade Gecko devices launched!

Hi,

 

Thanks for your interest!  I will relay your suggestion to our team that manages samples.  In the meantime, if you need more you can buy individual parts on the major web distributor sites, such as Digikey or Mouser.  I just checked and they are in stock at both.

 

Regards,

Ted

Posts: 4
Registered: ‎03-18-2015

Re: New EFM32 Pearl and Jade Gecko devices launched!

Hi,

I just obtain a development KIT

SLSTK3402A for PG12, but I don't know to install  any code examples for this KIT.

 

in folder

c:\SiliconLabs\SimplicityStudio\v4\developer\sdks\exx32\v4.4.1\kits\

 

are only subfolder SLSTK3401A_EFM32PG

Are there any code examples for this family chip?

 

Martin

 

 

Posts: 348
Registered: ‎02-26-2013

Re: New EFM32 Pearl and Jade Gecko devices launched!

Hi @MartinS,

 

v4.4.1 is an old version of the SDK that does not have the PG12 examples. I suggest updating or reinstalling Studio so that you have the newer Gecko SDK Suite.

 

Once updated, the PG12 examples will be located:

C:\SiliconLabs\SimplicityStudio\v4\developer\sdks\gecko_sdk_suite\v1.0\app\mcu_example\SLSTK3402A_EFM32PG12

 

If you still have issues, I suggest starting a new thread or submitting a support request (https://www.silabs.com/support > Email Support Request).

 

Posts: 4
Registered: ‎03-18-2015

Re: New EFM32 Pearl and Jade Gecko devices launched!

Hi,

thanks for info, now it works - I have already updated Simlicity, but SDK not. When I updated SDK too, I works and Examples are there.

I want to test examples with uVision5, but it not works. Compilation and link process is OK. When I try to debug I obtain error message "No Cortex-M SW-Device Found" (KIT 3502 in both Debug mode "MCU" and "IN").

Message in uVision5 in log space is suspicious:"* JLink Info: Device "ARM7" selected.", but PG12 is only CORTEX-M4.

Setting in Flash Download  Programming Algorithm is "EFM32 Wonder Gecko", because PG is not available.

How can I connect to KIT with PG12 from uVision5?

 

Martin

 

 

PS: uV5:

Toolchain:        MDK-ARM Standard Cortex-M only  Version: 5.13.0.0

Target DLL:             Segger\JL2CM3.dll      V2.99.11.0

Posts: 2,209
Registered: ‎10-14-2014

Re: New EFM32 Pearl and Jade Gecko devices launched!

i think you need check if the uv5 already support EFM32PG12. if not you need update it.
http://www.keil.com/dd2/
WeiguoLu
Posts: 53
Registered: ‎01-04-2010

Re: New EFM32 Pearl and Jade Gecko devices launched!

Support

PG12B and PG1B

Posts: 4
Registered: ‎03-18-2015

Re: New EFM32 Pearl and Jade Gecko devices launched!

Thanks for all. I updated KEIL for family PG12, but update of SEGGER driver was necessary too (for FLASH upload process). Now it works.

 

Martin

<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Super Star</font></font> </a> iwl
Posts: 5
Registered: ‎07-19-2017

Re: New EFM32 Pearl and Jade Gecko devices launched!

Can I just program it with Simplicity Studio and C like STK 3200?

 

I would like the much more Ram and Flash.

 

Posts: 2,209
Registered: ‎10-14-2014

Re: New EFM32 Pearl and Jade Gecko devices launched!

@iwl

Simplicity Studio should be ok to support EFM32PG and EFM32JG.

You could use Simplicity Studio to program and debug these device.

WeiguoLu