How to Connect to a Device and Upload the Flash Content with Simplicity Studio

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Master Employee</font></font> </a> delu on ‎04-13-2017 04:42 PM

Question

How do I connect to a device and upload the flash content with Simplicity Studio?

Answer

To read out the flash content of a device using the STK (J-Link):

 

  1. Connect the mini USB port to PC and start Simplicty Studio.
  2. In the launcher perspective (SS v4) or IDE perspective (SS v4 and v3), select Run->Connect to->Silicon Lab Arm part.
  3. For Simplicity Studio v4, be sure the Process under Debug view is selected,
  4. For Simplicity Studio v3, expand the Kit in debug view by clicking it, then select the part under the kit.
  5. Click the Memory->+ tab and select the target flash address range you need to view.