Converting Hex to Bin and Vice Versa

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Master Employee</font></font> </a> delu on ‎04-13-2017 04:50 PM

Question

Do you have a tool to convert a file image between bin and hex formats?

Answer

Yes. Use Simplicity Commander to convert between bin and hex formats.  Simplicity Commander is packaged with Simplicity Studio (www.silabs.com/simplicity).

 

The command to do this is demonstrated below:

 

C:\SiliconLabs\SimplicityStudio\v4\developer\adapter_packs\commander>commander convert aba.hex -o aba.bin
Parsing file aba.hex...
Writing to aba.bin...
DONE