Bankswitch disable bit in EFM32PG12

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero Employee</font></font> </a> marao on ‎06-09-2017 05:38 PM

Question

The Lock bits description section (6.3.2) in the reference manual of EFM32PG12 states the following about the bankswitch disable bit -

 

Capture.PNG

 

At what position is the Bankswitch disable bit?

Answer

The bankswitch disable bit is bit 0 of the configuration word One. If the value of this bit is 1, bankswitching is disabled.